Since I am new with this product any and all suggestions are welcome! We installed Code Composer 6 on a Windows 7 64bit PC with an i5 processor and 8.0Gigs of RAM. The first build of the day is approximately 45 seconds, which is acceptable. As I continue to modify, and need to rebuild the next will exceed 4.0 minutes plus (and will spike the CPU only) and increase as work/changes continue. If I reboot the system it will go right back to the 45 second rebuild time. Any settings/suggestions etc??
Thank you all in advance for your assistance!