Hi,
Am using CCS Version: 6.0.1.00040 ,
Am using CC3200 SDK 1.0.0
When I was compiling my application , just Adding One line of code UART print , Increased my binary size to 1 Kb . Why it is happening like this ? Can A single line of code can be 1 K and also if I remove some unused variables and functions Image size is not reducing much .
Image Size is very critical factor in my Application , How can I use efficiently my CCS ?
I tried all the optimisation levels in CCS , that didnt hel much ?
Thanks A Lot in Advance,
~Thanga Raj