Hello.
I'm new to CCS so please excuse my possible silly questions.
Case: We have a (CCS v5.5) project consisting of C++, C and ASM files for a F2806x MCU.
In the link map file I find the following (another company has included it's C++ code into the system, out of our control unfortunately):
GLOBAL SYMBOLS: SORTED BY Symbol Address
address name
-------- ----
00000000 __sys_memory
00000001 __SYSMEM_SIZE
00000001 __TI_args_main
00000050 __stack
00000100 ___TID_12PsuDriveCtrl
00000101 ___TID_6PsuApp
00000102 ___TID_17PsuSendSensorData
00000103 ___TID_12PsuAppTarget
00000104 ___TID_22SdaTreatmentController
00000105 ___TID_14SdaPowerSupply
00000106 ___TID_15SdpPackVariable
00000107 ___TID_16SdpPackParameter
00000108 ___TID_12SdpPackEvent
00000109 ___TID_11SdpPackData
0000010a ___TID_7SdpPack
0000010b ___TID_11SosItemList
0000010c ___TID_7SosItem
0000010d ___TID_11SosVariable
0000010e ___TID_16SosVariableFloat
0000010f ___TID_14SosVariableInt
00000110 ___TID_15SosParameterInt
00000111 ___TID_17SosParameterFloat
00000112 ___TID_12SosParameter
00000113 ___TID_8SosEvent
00000114 ___TID_11SosDataType
00000115 ___TID_7SosData
00000116 ___TID_7SosPort
00000117 ___TID_Q2_3std9type_info
00000380 __STACK_SIZE
000003d0 __STACK_END
00000880 _DevEmuRegs
00000985 _SysPwrCtrlRegs
. . .
At startup, the SP is set to 0x00000400.
But, all these __TID_xxxx sections are within the stack area...
Q-1: Should they be here?
Q-2: If so, could the be placed downwords to start at 0x50 (stack-area from 0x50 to 0x100 (0xB0=176 bytes are now/otherwise wasted/unused)
Q-3: if not, where in memory should the be placed?
Q-4: What are they?
I'll really appreciate assistance with this matter.
Best regards
terje bohler