Hello,
I use WIndows 7 64bits and CCS V6.1.0.00104 and want to try to debug my program with XDS510 USB emulator.
First step I tested on a Tiva board and use the internal debugger and all works well.
After that, I tested with my XDS510 USB Emulator on the same board and the programs start to be loaded but hang at 97 %:
I was thinking that it was due to the fact that I haven't got a valid licence for CCSV6 so I tried with a 90 day licence.
I can see that the licence is now Evaluation Licence with 87 days remaining:
But the problem remain the same, load hang at 97%...
I think it's a Licence issue, I also have a CCSV5 with a valid full licence and programs load without any problem with my Emulator.
I already tried to uninstall CCSV6 and reinstall, it always do the same...
Do you have any suggestion?
Thank you in advance for your help.
Regards,
Max.