I run a project on the CCS V6.1 .
I connect the Debugger DevpPack from which is XDS110 to a target board of SensorTag both from TI.
When I try to run on debbug mode I get this error.
Cortex_M3_0: Failed Board Reset
IcePick_C: Error connecting to the target: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed. The cause may be one or more of: invalid firmware update, invalid XDS110 serial number, or faulty USB connection. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the ReadMe.txt file there for instructions. (Emulation package 5.1.641.0)
So at first I go to the folder and make DFU again and it work.
Buteach time I go out of the debbug mode and get back it show this message again.
Does the fireware get lost every time or I do somthing wrong? It is not logical to make this proccess eah time
Bar.