I'm trying to load both a BSL and my application into an MSP430. In IAR there is an option to download extra images. Is there a way to do this with CCS? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm trying to load both a BSL and my application into an MSP430. In IAR there is an option to download extra images. Is there a way to do this with CCS? Thanks.
Lee,
IAR does have this functionality, but I do not think CCS does. If you have your .txt file already compiled, you can use the MSP430Flasher or the Elprotronics LiteFET-Pro430 tool as well to load them. If you are looking for a production programming solution, the MSP-GANG will also load up to 8 devices with .txts
For a more definitive answer if CCS has this ability, I will move this post to the CCS forum for that answer.
Regards,
JH
I'm trying to load multiple images into the device. Can I do this with MSP430Flasher? I've looked through the documentation but I don't see anything about loading multiple files..
Regards,
Lee
Lee,
I have been informed form the CCS team that CCS does not support multiple image downloads.
As for MSP430Flasher, that use-case would have to be more along the lines of what old_cow_yellow was commenting on.
Regards,
JH