from following site
https://dev.ti.com/pinmux/app.html#/config/AM335x/ID_500/ID_0/null/null
I'm add the uart.
uart rx option is all checked & disabled without txd.
Is it correct?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
from following site
https://dev.ti.com/pinmux/app.html#/config/AM335x/ID_500/ID_0/null/null
I'm add the uart.
uart rx option is all checked & disabled without txd.
Is it correct?
Hi,
The link you have posted is not working.
Ahn,
Your assertion that the signal is output is correct. However, based on the comments (see below ) from the engineer with more in depth device knowledge it should have no impact on the generated code. We'll fix the UI issue in the next release of tool to avoid this confusion.
"However, the customer can safely ignore this. The “RX” configuration in the pinmux tool controls the Pad Config register’s RXACTIVE bit. This bit only enables/disables the pad receiver circuitry. It’s not a direction bit. A pad can be configured as an output with receiver enabled. "
Thanks,
Mandeep Deol