Hello,
Compiling our project with Code Composer Studio 5.5.0 yiels a warning "#16004-D file". I couldn't find any information what it means or what it stands for. Could you please help me?
Thank you in advance and best regards
André Niederlein
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Compiling our project with Code Composer Studio 5.5.0 yiels a warning "#16004-D file". I couldn't find any information what it means or what it stands for. Could you please help me?
Thank you in advance and best regards
André Niederlein
Found the thread https://e2e.ti.com/support/embedded/tirtos/f/355/t/365540 which suggests the problem is that the compiler version 5.1.1 in use is "too old", and than upgrading to compiler 5.1.5 or later will resolve the incompatibility.Andre Niederlein said:'Flags: -mv7R4 --code_state=32 --float_support=VFPv3D16 --abi=eabi -O0 --opt_for_speed=3 -g --define=__STDC_LIMIT_MACROS --define=FUMU --diag_warning=225 --diag_warning=16004 --display_error_number --enum_type=packed --printf_support=full -z -m"BOARD_FUMU1.map" --heap_size=0x800 --stack_size=0x800 -i"C:/ti/ccsv5/tools/compiler/arm_5.1.1/include" -i"C:/ti/ccsv5/tools/compiler/arm_5.1.1/lib" -i"C:/Projekt_Workspace/projekt.cu_application/vendor/F021FlashAPI" --reread_libs --define=SAFERTOS_DEMO_APP --warn_sections --xml_link_info="BOARD_FUMU1_linkInfo.xml" --rom_model --be32'
"C:/ti/ccsv5/tools/compiler/arm_5.1.1/bin/armcl" -@"ccsLinker.opt" -o "BOARD_FUMU1.out"
<Linking>
warning #16004-D: file
"C:/Projekt_Workspace/projekt.cu_application/vendor/F021FlashAPI/F021_API_Co
rtexR4_BE_V3D16.lib<Async.obj>" has a Tag_PCS_config attribute value of "1"
that is different than one previously seen ("0"); combining incompatible
files