I have an XDS100v2 USB emulator that I am trying to use to program a TM4C1294NCPDT. When ever I try to debug the program I get the following error message:
CORTEX_M4_0: Error connecting to the target: (Error -1141 @ 0x0) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.73.0)
I am using CCS v5.4.0 on a Windows 7 Professional computer.
When I use Test Connection it returns that the JTAG IR Integrity scan-test has succeeded.
Below is an image of the advanced target configuration window with the settings I am trying to use to connect.
Does anyone know what can be causing this error and how can I fix it?