Hi,
I am able to write the code to flash in DSP 28335 using XDS100V2 JTAG emulator. However, I am not able to obtain the real time values while the JTAG is still connected .
First, I debugged the program which automatically writes the code in flash. Then as shown in picture, the debug window appears. After that ,I click the R-click and connect to TARGET, but i get an error message (as shown in second image) "No source available for 0x3ff9ce" and the XDS100V2 debug probe status is shown to be "SUSPENDED".
I am not able to understand why i am unable to obtain the retrieve real time values while JTAG is connected.
Some threads suggest to go to RUN--Load the program; but that doesnot help either.
Any help is appreciated.Doc1.pdf
Thank you,
Ujjwal