Dear TI representative,
Attached there are images describing my issue. Important parts on the images are highlighted in yellow.
Image #1: After creating my Target Configuration File for my AM3359 processor, I search for my GEL file, and add it as an initialization script.
Image #2: Then when I launch the target configuration file, CCS 6.0.1 crashes and exits.
NOTE: CCS only crashes when I add an “initialization script” like on image #1. But if I lunch the target file without initially adding a GEL (i.e., I launch the target configuration file first, then I go to “Tools > GEL Files” and add the GEL file manually, unlike on image #1), then the program does not crash.
Image #3: I’ve found when the issue happens. When I import my target configuration file, and select “Copy file,” CCS tries to look for the Target Configuration file in the wrong path. But when I do “Link to files” and I launch the target configuration with the GEL already imported, then the program does not crash anymore. Why does this happen?
Also, the sentence “Select show files should be imported:” on image #3 seems to have the word “show” instead of “how”?
Thanks