Hi
I am trying to collect data with a CC2650STK and am using the CCS studio to run the debug, I am unable to fine the node required for node RED to all communication between the sensor tag and the CCS studio
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can you explain what you are trying to do with CCS?
The work we've done involved a linux board (beaglebone) running a nodejs script that communicates to the sensortag via bluetooth and via MQTT to the IBM server running node red.
The instructions to set up the board are at
CCS can be used to compile and debug the application on the CC2650.
Iain
The SensorTag Smartphone iOS/Android Apps (www.ti.com/.../sensortag) as well as the AM335x based BeagleBone sensortag gateway (developer.ibm.com/.../ti-beaglebone-sensortag) both send SensorTag sensor data via MQTT protocol to IBM's Internet of Things Foundation Cloud service (IoTF). By default, these are configured to use IBM's public MQTT 'QuickStart' broker, enabling data to be viewed using the publicly accessible visualiser (quickstart.internetofthings.ibmcloud.com).
This data can also be also be processed using a Node-RED flow, running inside an IBM Bluemix instance (for example). The easiest way to configure Node-RED to connect to the IBM IoTF service and collect data from devices is to use the "ibmiot" input node, configuring the properties of the node to specify the corresponding Device ID of the SensorTag.
The following video provides a walk-through of the SensorTag and an example of processing data from a SensorTag using Node-RED.
http://www.element14.com/community/events/4282
Hope this helps,
~roger