This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error in CDT Core during AST creation

Hi,

I have Code Composer Studio 5.5.0.00077 and when I add a new driver files to my project (.h and .c) and try to save as I make changes I get an error.

Windows Vista Service Pack 1

I added them in Code Composer (File->New-> Source File, and File->New->Header File).  Also tried select and drag from Windows file explorer to Code Composer Studio project.

"C/C++ Indexer has encountered a problem.

An internal error occurred during: "C/C++ Indexer".

Looking at the Error Log I see:

1. An internal error occurred during: "C/C++ Indexer".

2. Error in CDT Core during AST creation

3. Problems occurred when invoking code from plug-in: "org.eclipse.cdt.core".

Only the new files cause these errors in the Error Log.  The original files in this project do not.

In Code Composer I just click in the file and I get these Errors (2, 3).

Any help is appreciated.

Regards,

Ed