Hello,
i am using CCS V3.1 and, and i want to generate code which will be directly downloaded onto DSP 6713 (no emulator, no simulation...). I use SpectrumDigital DSK6713 and set up C6713 DSK-USB in the code composer studio setup.
The problem is that the .out file that is generated contained profiling information. For example, in one of the .asm file:
1 ;******************************************************************************
2 ;* TMS320C6x C/C++ Codegen PC v5.1.0 *
3 ;* Date/Time created: Mon Jul 27 20:07:30 2015 *
4 ;******************************************************************************
5 .compiler_opts --endian=little --mem_model:code=far --mem_model:data=far --predefine_memory_mo
6
7 ;******************************************************************************
8 ;* GLOBAL FILE PARAMETERS *
9 ;* *
10 ;* Architecture : TMS320C671x *
11 ;* Optimization : Enabled at level 3 *
12 ;* Optimizing for : Speed *
13 ;* Based on options: -o3, no -ms *
14 ;* Endian : Little *
15 ;* Interrupt Thrshld : Disabled *
16 ;* Data Access Model : Far *
17 ;* Pipelining : Enabled *
18 ;* Speculate Loads : Disabled *
19 ;* Memory Aliases : Presume are aliases (pessimistic) *
20 ;* Debug Info : Optimized w/Profiling Info *
21 ;* *
22 ;******************************************************************************
The question i had is : how remove profiling information and just generate an executable code which will be put in production ? Is the target i chose is not the good one ("C6713 DSK-USB") ?
Thank
Sébastien