Hİ
I am trying to learn how to use SD card controller of C5515 and decided to use CSL 3.04. I successfully compiled and run the CSL example project. As next step, I created a new project which is called SDCardTrial in my workspace and try to call CSL functions in this project. And this is where my problems started. I dealed with lots of problems and solved some of them but i couldnt solve this linker problem. My console output, necessary information and screenshots can be seen below:
CCS Version: 6.1.0.00104
Compiler Include Settings:
Linker File Search Path Settings
Console Output:
**** Build of configuration Debug for project SDCardTrial ****
"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k all
'Building file: ../main.c'
'Invoking: C5500 Compiler'
"C:/ti/ccsv6/tools/compiler/c5500_4.4.1/bin/cl55" -v5515 --memory_model=large -g --include_path="C:/ti/ccsv6/tools/compiler/c5500_4.4.1/include" --include_path="C:/ti/bios_5_42_00_07/packages/ti/bios/include" --include_path="C:/ti/bios_5_42_00_07/packages/ti/rtdx/include/c5500" --include_path="C:/c55_lp/c55_csl_3.04/c55xx_csl/inc" --include_path="C:/Users/Hasan/NewWorkSpace/SDCardTrial/Debug" --define="_DEBUG" --define=c5515 --display_error_number --diag_warning=225 --ptrdiff_size=16 --algebraic --preproc_with_compile --preproc_dependency="main.pp" "../main.c"
'Finished building: ../main.c'
' '
'Building target: SDCardTrial.out'
'Invoking: C5500 Linker'
"C:/ti/ccsv6/tools/compiler/c5500_4.4.1/bin/cl55" -v5515 --memory_model=large -g --define="_DEBUG" --define=c5515 --display_error_number --diag_warning=225 --ptrdiff_size=16 --algebraic -z -m"SDCardTrial.map" --stack_size=0x200 --heap_size=0x400 -i"C:/ti/ccsv6/tools/compiler/c5500_4.4.1/lib" -i"C:/ti/ccsv6/tools/compiler/c5500_4.4.1/include" -i""C:/ti/bios_5_42_00_07/packages/ti/rtdx/lib/c5500" -i"C:/ti/bios_5_42_00_07/packages/ti/bios/lib" -i"C:/Users/Hasan/NewWorkSpace/C55XXCSL_LP" -i"C:/Users/Hasan/NewWorkSpace/SDCardTrial" -i"C:/ti/ccsv6/tools/compiler/c5500_4.4.1/lib" --reread_libs --display_error_number --warn_sections --xml_link_info="SDCardTrial_linkInfo.xml" --rom_model --sys_stacksize=0x200 -o "SDCardTrial.out" "./main.obj" "../C5515.cmd" -l"Debug/C55XXCSL_LP.lib" -l"rts55x.lib" -l"libc.a"
<Linking>
fatal error #10009: no input files
>> Compilation failure
gmake: *** [SDCardTrial.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
I make sure that all the build variables are defined correctly, and make sure that all the lib files are in the given directories.
Any help will be much appreciated.
Thanks in advance.
Hasan