Hey everyone !
I have my application, with work perfectly, based on few sensortags. Now i want a sensortag to be in debug mode, with printf everywhere (i already made the "debug firware") link onto the Rpi (but could be any linux based computer).
I just want my linux ((actually, raspbian) to read the serial port and to save it in a txt file.
How can i do that. I tried, i was not even able to detect witch serial port was used...
EDIT : I tried
cat /dev/ttyS*
-> no port worked (just in case it is useful, i have ttyS0 to ttyS31)
Then i tried :
lsusb
output :
Bus 001 Device 002: ID 8087:8000 Intel Corp. Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub Bus 003 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub Bus 002 Device 003: ID 0bda:5727 Realtek Semiconductor Corp. Bus 002 Device 002: ID 17ef:6022 Lenovo Bus 002 Device 007: ID 0451:bef3 Texas Instruments, Inc. Bus 002 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
then
sudo modprobe usbserial vendor=0x0451 product=0xbef3
Now it is enabled onto /dev/ttyUSB1, but it still does not work, neither putty, nor the
cat /dev/ttyUSB1
reads something (but the link is opened without errors)