Hi,
I have previously CCS v5.5.0 installed. I have to upgrade it to CCS v6.0 to work with CC2650 but I have hard luck in doing so. Apparently what I get from the installation log that it fails in installing FTDI drivers.
Executing c:/ti/ccsv6\utils\bin\DPInst64.exe /sw /sa /path "c:/ti/ccsv6\ccs_base\emulation\drivers\cc3200\ftdi"
Script exit code: unknown signal
Script output:
Script stderr:
child killed: unknown signal
Error running c:/ti/ccsv6\utils\bin\DPInst64.exe /sw /sa /path "c:/ti/ccsv6\ccs_base\emulation\drivers\cc3200\ftdi" : child killed: unknown signal
Unable to install FTDI drivers unknown signal
[22:30:36] dpinst return code = unknown signal
I have used the uninstalled from FTDI to clean any traces of previously installed FTDI drivers but still no luck. I am using Windows 7 64-bit.