Hi,
We currently use CCS 3.3 to develop code for our C6201 and C6455 based boards using genuine XDS560 PCI and XDS510 ISA (remember them!) emulators. We've also got several Chinese knock off USB 510 type emulators that can sometimes be persuaded to work with the C6201, but I've never got them to work with the C6455.
We've recently bought a genuine Spectrum Digital XDS100V2, and downloaded and installed CCS 6. I've got that working on the C6455, but there doesn't seem to be any support for C6201. So my questions are:
1) What is the latest CCS that I can use to support C6201?
2) Is there a way to support both C6201 and C6455 using a USB type emulator - and if so what version of CCS and emulator do I need.
Cheers
Malcolm