Hi,
I'm trying to get Code Composer 6 installed on Ubuntu 14.04. I've followed the directions from the wiki but after calling the installer the program just returns to the shell. I have installed the 32 bit libraries mentioned in the wiki.
otto@AFLAB2369297:~/Downloads/CCS$ lsb_release -a No LSB modules are available. Distributor ID: Ubuntu Description: Ubuntu 14.04.2 LTS Release: 14.04 Codename: trusty otto@AFLAB2369297:~/Downloads/CCS$ uname -a Linux AFLAB2369297 3.16.0-45-generic #60~14.04.1-Ubuntu SMP Fri Jul 24 21:16:23 UTC 2015 x86_64 x86_64 x86_64 GNU/Linux otto@AFLAB2369297:~/Downloads/CCS$ sudo apt-get install libc6:i386 libx11-6:i386 libasound2:i386 libatk1.0-0:i386 libcairo2:i386 libcups2:i386 libdbus-glib-1-2:i386 libgconf-2-4:i386 libgdk-pixbuf2.0-0:i386 libgtk-3-0:i386 libice6:i386 libncurses5:i386 libsm6:i386 liborbit2:i386 libudev1:i386 libusb-0.1-4:i386 libstdc++6:i386 libxt6:i386 libxtst6:i386 libgnomeui-0:i386 libusb-1.0-0-dev:i386 libcanberra-gtk-module:i386 gtk2-engines-murrine:i386 Reading package lists... Done Building dependency tree Reading state information... Done gtk2-engines-murrine:i386 is already the newest version. libasound2:i386 is already the newest version. libatk1.0-0:i386 is already the newest version. libcanberra-gtk-module:i386 is already the newest version. libdbus-glib-1-2:i386 is already the newest version. libgconf-2-4:i386 is already the newest version. libgdk-pixbuf2.0-0:i386 is already the newest version. libgnomeui-0:i386 is already the newest version. libice6:i386 is already the newest version. libncurses5:i386 is already the newest version. liborbit2:i386 is already the newest version. libsm6:i386 is already the newest version. libusb-0.1-4:i386 is already the newest version. libusb-1.0-0-dev:i386 is already the newest version. libx11-6:i386 is already the newest version. libxt6:i386 is already the newest version. libxtst6:i386 is already the newest version. libc6:i386 is already the newest version. libcairo2:i386 is already the newest version. libcups2:i386 is already the newest version. libgtk-3-0:i386 is already the newest version. libstdc++6:i386 is already the newest version. libudev1:i386 is already the newest version. The following packages were automatically installed and are no longer required: linux-headers-3.16.0-30 linux-headers-3.16.0-30-generic linux-image-3.16.0-30-generic linux-image-extra-3.16.0-30-generic Use 'apt-get autoremove' to remove them. 0 upgraded, 0 newly installed, 0 to remove and 0 not upgraded. otto@AFLAB2369297:~/Downloads/CCS$ chmod +x ccs_setup_6.1.0.00104.bin otto@AFLAB2369297:~/Downloads/CCS$ ./ccs_setup_6.1.0.00104.bin otto@AFLAB2369297:~/Downloads/CCS$
Are there other dependencies that I am missing?
Thanks!