Problem: When I attempt to import an existing project (created in CCS 5) to my current workspace (Recently Updated CCS 5.5) I get the following error:
An internal error occurred during: "C/C++ Indexer". java.lang.NullPointerException
My coworker was able to import the project no problem into CCS 5.2, so I tried doing a clean install of 5.2 on my PC, but still ran into the same issue (I performed another clean install back to 5.5 afterwards). We are both running Windows 7 SP1 and our computers are almost identical in terms of hardware, so I figured there must be something about my CCS install that is giving me trouble.
I noticed on the forums that other people have had similar problems when trying to import their projects, but I did not see anyone with this indexer error when attempting to import an existing CCS5 project (I think there was a similar one where they were attempting to import a CCS4 project, but it did not get resolved completely) so I figured I would post here and see if anyone has a solution.
My exact CCS Version is: 5.5.0.00077, and this project was developed for a Piccolo TMS320F28067 DSP.
I am attaching screenshots of the error as it occurs, as well as my indexer settings. I have a zip file of my install_logs directory, but I am not exactly sure how to attach it to this post.
Please let me know if there are any other files or pieces of information I can provide to help finding a solution. As long as they don't contain any proprietary information, I will be happy to share them.