Hello
I installed CCS6.1 on an Ubuntu 15.04, x64 platform with the latest sysbios, xdctools, and am335x sdk (same as I have on a Windows 7 host). I created and compiled a simple "hello world" application. The debugger fails to find the eval board's XDS100v2 debug probe -- the same AM3359 ICE v1 eval board that I use to test the Windows 7 system.
The Error message I see is:
Error connecting to the target:
(Error -151 @ 0x0)
One of the FTDI driver functions used during
the connect returned bad status or an error.
The cause may be one or more of: invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
(Emulation package 6.0.14.0)
"strace xds100serial" shows that xds100serial is searching /sys/bus/usb/devices for its XDS100 probe, but in 15.04, the probe appears under /sys/bus/usb-serial/...
Please advise.
Regards,
-david