Hello
I use windows 7 , and installed CCS 6 .
Was writing code and all was OK , program was compiling and there was no any problems with level of optimization off. Once I coudn`t add in program delay_loop . Linker don`t let me to add it. I getting error - errors encountered during linking. I tried to change levels of optimizations but never any results.
Program is compiling and linker don`t swears. But when I launch program, all delay_loop s and - for (i = 0; i < 10000; i++) {} in program (with level of optimization 0,1,2,3,4) is skiped .Please help me. By my mind some memory of chip is full. But if this is so how to clear it. I tried by flash eraser but it only clears flash sectors. Here I`m adding screenshots. Thank you very much.
And here is memory allocation screenshot