I have CCS Version: 6.1.0.00104
When I click on New Project, the dialogue box asks for the Target. The target is a C6000 family DSP, but this option (or any C6xxx) is not available in the drop down list.
What should I do?
Much Thanks,
G
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have CCS Version: 6.1.0.00104
When I click on New Project, the dialogue box asks for the Target. The target is a C6000 family DSP, but this option (or any C6xxx) is not available in the drop down list.
What should I do?
Much Thanks,
G
Looking at a CCS 6.1.0.00104 installation for which all support for all device families was installed shows support for the TMS320C6701, TMS320C6727 and TMS320C6713 processors.Gi Gi said:Using the C6701 or C6727. Do I need to purchase C6x support? If I get the TMDSDSK6713 dev kit, will that have CCS C6x support?
If your CCS installation isn't showing support for any C6xxx devices, this probably means that during the CCS installation the C6xxx product families were not selected to be installed.
If you re-run the CCS installer and point to the existing installation directory, on the Processor Support dialogue if you tick the "C6000 Single-core Device Support" and "TI C6000 Compiler" options that should add support for C67xx devices: