Hi there,
I have this problem just on one computer, the others work fine. So CCS5.5 originally had xdctools 3.24.7.73 but when I added a GRACE project which was using xdctools 3.25.3.72 I had a error:
xdc.tools.configuro: InternalError: ti.platforms.msp430: can't resolve name xdc.platform.IPlatform.peripherals
and also a message that I have to add a new version of xdctools. When I installed a required tool CCS could not recognize a new addition even if I pointed that this folder is a new XDCtools though the RTSC window. Read some stuff on forum trying to resolve the problem but it appears that only re-installing CCS can help out.
So are there any other options to get it worked? Just do not want to reinstall CSS, too much headache.
Thank you
Stan