Hello,
I had imported (with copy) a project into a new workspace yesterday. Today, while comparing the .cproject files from the original project and the one that was copied, I noticed a new string macro named {ORIGINAL_PROJECT_ROOT} had been created in the copied project's .cproject file and the string macro value is equal to the original project directory.. Also, the original macro, {PROJECT_ROOT}, was replaced by {ORIGINAL_PROJECT_ROOT} in all the include paths.
Why isn't CCS using the copied project's root directory as a basis for its include paths?
Thanks,
Stephen