Hi,
I have the following requirement,
1) i would like to power up the micro controller before i begin the test case execution, complete the test execution and at the end power down the micro controller.
I would like to do the power up/down via .js script files, either through calling a external .js or internally in the same script by writing certain commands.
Please help me if there is any way to accomplish this.
Microcontroller (TIVA C series) - is powered with external power source.
Any mechanism or approach to either communicate to the external power source or turning off/on the power internally should be good.
2) In certain test cases i would like to write a particular memory location and then wait for certain time, such that
software running on the controller reads the (written value) and perfroms the computation and then i want to measure
or monitor the updated value after some time (say 5 seconds)
Please help me with this as well.
Thanks,
-Nikhilesh