For my big confusion, CCS is the first development tool with which I failed to build an 'out of box' example.
First I tried on Windows, but it just failed to start with an error message advising to look at 'null' log file.
Not a big surprise, though. Then I installed a Linux version getting various errors on the way.
But finally it runs and I even managed to import an example. But it does not compile with a fatal error #10009: no input files
Even on-line version is 'half-working'. To work with it I am using two browser, Chrome an Firefox, because some features works in Chrome and do not in Firefox and vice versa.