I am working in Code Composer Version: 6.1.1.00022 with Guicomposer 6.1 trying to bind to data in a Tiva TM4C1294KCPDT. I can Bind a char array "labels" or int array "testdata" to the field column names and it will display properly but... if I bind labels to the column names and testdata to the data field the labels will display but instead of data all that shows is lines or empty cells. Could you please let me know what I am missing. I've search for info on dgrid but it seems very limited.
Also if this does work properly would you then be able to edit these cells which would then update on the target as the textbox does?
I see you can export this data to a file would you also be able to import a file to update the target?
This would be a big help to download a set of parameters to the target.
Thank you, Dan