In a nutshell when I attempt to import an existing CCS project into a new workspace the project does not appear in the "Discovered Projects" pane in the
"Select CCS Projects to Import" dialog.
Here are the steps I took.
- Created a completely new CCS workspace
- Created a new CCS project of type "empty Project (with main.c)"
- Added source file directories with the "copy into project" option selected.
- Added my main.cpp into the project directory.
- Modified Include dirs in the project preferences as appropriate.
- Verified that it builds fine.
- Commit project directory to our SVN repository.
- Check out the project from SVN into a new directory.
- Create a new CCS workspace
- Attempt to import "CCS Project" into the new workspace
...empty list of projects to select from as described in the beginning of this issue.
I have tried several variations of the above using an existing project and none of them worked.
Does anyone have any ideas?
Victor