Hi,
I have CCS for Mac OS X latest version (6.1.1.00027) installed. Originally, it wouldn't recognize the MSP-EXP430FR5739 board at all. Then I installed the LPCDC drivers from the Energia website, and am able to at least use the application UART on the board.
On plugging in, the Console shows:
26/11/15 12:12:26.000 kernel[0]: 0 0 dgmdmcontrol: start - Failed to find the CDC driver
26/11/15 12:12:26.000 kernel[0]: ----------------------------------------------------
26/11/15 12:12:26.000 kernel[0]: Texas Instrument LaunchPad / EZ430-RF2500 CDC/ACM Driver
26/11/15 12:12:26.000 kernel[0]: Version 1.0.3b - Terence Ang 2011
26/11/15 12:12:26.000 kernel[0]: ----------------------------------------------------
26/11/15 12:12:26.000 kernel[0]: Device Name = Texas Instruments MSP-FET430UIF
26/11/15 12:12:26.000 kernel[0]: Serial Number = 12FF50DCF9982F5F
26/11/15 12:12:26.000 kernel[0]: ----------------------------------------------------
26/11/15 12:12:26.000 kernel[0]: MSP430LPCDC : Version number - 1.0.3b, Input buffers 8, Output buffers 16
Is this a known issue? Am I supposed to be able to use the MSP-EXP430FR5739 board with CCS for Mac OS X (El Capitan latest version)?