Hi,
Im very new to use CCS and Energia both. I am using CCS v6 and energia-0101E0016. I have OS-X 10.10.5. I'm new in using mac as well.
Problem:
I can find Energia Sketch Import option under Project -->
The I get the searching window to add the path of energy -->
Then I Browse and add the Application folder where the executable is (I think, if I am not wrong, cause using mac for the first time as well) -->
But then it says that " The selected directory does not resemble an Energia install. Please select the directory containing the 'energia' executable", and I cannot go Next -->
So thats the problem. Can anyone help me please?
Thanks in Advance.