We're attempting to run a command line nightly build on a Windows 7 Pro SP1 machine with CCS 6.1.1.00022 and the build appears to complete successfully but eclpsec is returning 1 as though it detected an error. Am I missing something or is the eclipsec return value not useful in determining success or failure. The output of the linker command, along with the value of %ERRORLEVEL%, is below if it matters. Thanks.
'Invoking: C2000 Linker'
"C:/ti/ccsv6/tools/compiler/ti-cgt-c2000_6.4.6/bin/cl2000" -v28 -ml -mt --float_support=fpu32 --tmu_support=tmu0 --cla_support=cla1 --vcu_support=vcu2 -O2 --define=_INLINE --define=RELEASE --define=FLASH --define=CPU1 --diag_warning=225 --display_error_number --diag_wrap=off -z -m"28377S_MCB.map" --stack_size=0x200 --warn_sections -i"C:/ti/ccsv6/tools/compiler/ti-cgt-c2000_6.4.6/lib" -i"C:/ti/ccsv6/tools/compiler/ti-cgt-c2000_6.4.6/include" --reread_libs --display_error_number --diag_wrap=off --xml_link_info="28377S_MCB_linkInfo.xml" --rom_model -o "28377S_MCB.out" "./DLOG4CHC.obj" "./F2837xS_CodeStartBranch.obj" "./F2837xS_DefaultISR.obj" "./F2837xS_EPwm.obj" "./F2837xS_GlobalVariableDefs.obj" "./F2837xS_Gpio.obj" "./F2837xS_PieCtrl.obj" "./F2837xS_PieVect.obj" "./F2837xS_SysCtrl.obj" "./F2837xS_usDelay.obj" "./HardwareInit.obj" "./MCB_ISRs.obj" "./SPIcomms.obj" "./main.obj" "../2837xS_FLASH_IQMATH_lnk_cpu1.cmd" "C:/ti/controlSUITE/device_support/F2837xS/v160/F2837xS_headers/cmd/F2837xS_Headers_nonBIOS.cmd" -l"libc.a"
<Linking>
'Finished building target: 28377S_MCB.out'
' '
**** Build Finished ****
================================================================================
CCS headless build complete!
******************************************************************
* Release build return error code of 1
******************************************************************