This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The configuration of the graph tool is really dependent on your application and how you want to visualize so we cannot give precise answers.
The CCS Online Help has some information on each of the fields for configuring the graph. Also this wiki page has some interesting details. Hope this helps!
Thanks Aarti, I will make myself clear about the issue I am facing with the graph tool.
In the motor control based project for BLDC motor control using DRV8312-69M kit and TMS320F28069M control card, I want to plot few variables which are crucial for my estimation namely the motor voltages, phase currents. Now these are declared in the code as _iq format which shows that it is of long datatype as shown below. MATH_vec3 is a vector of 3 elements whose individual ones are _iq too. In the watch window, a Q24 format is used to visualise, which gives accurate results when seen in the watch window.
typedef struct _HAL_AdcData_t_
{
MATH_vec3 I; //!< the current values
MATH_vec3 V; //!< the voltage values
_iq dcBus; //!< the dcBus value
} HAL_AdcData_t;
When i want to graph one of the phase currents (preferably such as gAdcData.I.value[0] where gAdcData is a object defined), in the graph properties I provided the Q_value as 24, appropriate buffer size etc. For DSP datatype, I have no clue about which I'm supposed to provide. Variable being long datatype, I don't know if it's 32 bit, 16 bit etc (As per my knowledge size of long depends on processor). Could you help me out in this regard.
PS: I am asking about this because I can't quite see a comparable result between the graph window and actual expected waveforms with any of the possible Dsp datatypes.