Hi there,
, and the schema file found at C:\ti\ccsv6\eclipse\plugins\com.ti.ccstudio.project.templates_6.1.1.201508201800\schema
However, I am note sure if i can use project specs for my targeted use case:
- support multiple build configurations
- support including some files in a single build config but not another
- support different include paths and compiler defines
Is this possible using a project spec file? If so, what is the syntax for stating that some options belong to one config and others belong to a different config.