Hello while debugging code Launchpad do not connect. While testing connection of debugger it shows,
[Start: Texas Instruments XDS110 USB Debug Probe_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\Edison\AppData\Local\TEXASI~1\CCS\
ti\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioxds110.dll'.
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-448' (0xfffffe40).
The title is 'SC_ERR_VARIABLE_VALUE_SPELL'.
The explanation is:
Invalid spelling of the value of a configure variable.
[End: Texas Instruments XDS110 USB Debug Probe_0]
Please help me. What I have to do?