We need to implement / run 2 or more application simultaneously from cc2650. But when we try to flash more than one application, the memory of the flash exceeds. Hence we are able to flash only one application.
But when we got the LaunchPad cc2650 board we were able to do all the application with the firmware which was present in it by default.