I am encountering a bug in my firmware that causes the cc26xx to stop executing and simply hang. The bug goes away when I specify that CCS debugger config should disable all interrupts.
How do I find out what exceptions are being fired using CCSv6, provided that the cc26xx is connected via a USB XDS110 devpack debugger? Do I have to set a breakpoint in every single exception handler? Is there a better way?