I had an installation of CCS6 (6.1.1) which was working fine - but gave errors whenever it tried to do software updates. After trying to fix this for some time - I eventually installed a new version of CCS6 (6.1.3). However - when I first built my Motorware project - I got a warning:
"Description Resource Path Location Type
This project was created using a version of compiler that is not currently installed: 6.2.3 [C2000]. Another version of the compiler will be used during build: 15.12.1.LTS. Go to 'Help > Check for Updates' page to check for updates and visit <a href="liveaction:OpenAppCenter">CCS App Center</a> to get the latest compilers. Go to 'Help > Install New Software...' to install older compilers. Alternatively, migrate the project to one of the available compiler versions by adjusting project properties."
I have changed the project properties/general/compiler version so I no longer get this warning - but now the code it builds doesn't ruin correctly. The project builds without error - but the motor doesn't run. I suspect it has something to do with FPU floating point handling.
I have reverted to the old CCS with the original compiler and built the exact same project and the code builds and runs fine.
I have tried the suggestion "Check for updates" and this has not solved the problem.
Can anyone tell me what I need to do to make the project compatible with the new compiler? Or any other suggestions how to get a fully working version of CCS?
Thanks
Richard.