It seems when I attempted to update the XDS2xx firmware (1.0.0.2) on my K2E EVM, it failed and I am no longer able to communicate with it. At this moment I do not wish to return my K2E EVM, so I'm wondering about other options.
1) Can I load firmware on the CPLD via another method?
2) I own a Spectrum Digital XDS200 probe, To use this I seem to need a MIPI 60 connection. Sources for an adapter to connect it?
3) I have Xilinx tools and JTAG probes, Is there an image that I can load directly to the device?
Thanks in advance for the guidance,
Larry