Is there a mac version of UniFlash? Will the linux version run in the mac terminal? If not, What is the best way to flash a C2000 processor from the mac if I do not have access to the project file (it is being compiled on another machine)?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there a mac version of UniFlash? Will the linux version run in the mac terminal? If not, What is the best way to flash a C2000 processor from the mac if I do not have access to the project file (it is being compiled on another machine)?
Thanks
Neil,
The next version of Uniflash will support Mac. If you want to try it out, send me an email using the address in my profile.