This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS V6.1.3 Installation - missing message box

After we have started the offline installer it takes about 10-15 minutes until we get the check box to confirm the license agreement.

Because we get only messages at the start because of the antivirus program and then such long time no message on the screen it is confusing.

The installation files are located on local hard disk (files from CCS6.1.3.00034_win32.zip, 743.551.475 Bytes).

We are using Windows 7 Enterprise 64bit SP1 and Trend Micro Officescan, which cannot be turned off by the user.

We didn't notice this installation issue with versions <= V5.3.

Best regards

Joerg