We have just recently created a new product using the AM5728, Sys/Bios and CCS v6.1.1, CGT V8.1.0.
However, we also continue to support older products that were based on C6748 and C6482, using Dsp/Bios, CCS v5.5, CGT v7.4.5.
With an earlier version of CCS, V6.0.1 I believe, we were able to use the v7.4.5 compiler and build our projects and get the same exact output products.
However, now with CCS v6.1.1, when I try to import a legacy project I get this:
This project was created for a device not currently supported: TMS320C67XX.TMS320C6748. Check for updates and visit the <a href="liveaction:OpenAppCenter">CCS App Center</a> to get the latest device support, or migrate the project to closest matching supported device by adjusting project properties.
Our CM group will need to be able to build both the new and the legacy products. I don't want to have to tell them they need two different physical machines, but that seems like the only answer.
What options do you suggest for moving forward with this issue?