Hello,
my system configuration is:
Windows 8.1 64 bit
CodeComposer Studio v6.1.3 build 00034
The installation fails with the error:
Executing C:\ti/ccs_base/emulation/windows/DPInst64.exe /sw /sa /path "C:\ti/ccs_base/emulation/drivers/cc3200/ftdi" Script exit code: 512 Script output: Script stderr: Program ended with an error exit code
We have already made the following attempts in order to correct the previous error with no success:
- Maual installation of dpinst64.exe .
- Copy and paste of the following libraies to C:\Windows\System32 folder:
C:\Windows\System32\ftbusui.dll
C:\Windows\System32\ftd2xx.dll
C:\Windows\System32\FTLang.dll
C:\Windows\System32\drivers\ftdibus.dll
C:\Windows\SysWOW64\ftd2xx.dll
Any advise is welcome.
Thank you in advance.