Hello,
I've upgraded the compiler from 7.4.11 to 7.4.19 in CCSv5.5 using Check for Updates and now whenever I build from command line, compilation seems to pause randomly until I press Enter key (most likely closer to linking stage). This was observed also on CCSv6.0 on a different computer.
The makefile that I'm using is using shell=sh.exe which is available in system environment path (set path=%path%;C:\ti\ccsv5\utils\cygwin) and building the project is done via importing projects into workspace then calling CCSv5.5 to build the projects:
/ti/ccsv5/eclipse/eclipseC -noSplash -data ccsWorkspace -application com.ti.ccstudio.apps.projectImport -ccs.location "<my project>"
/ti/ccsv5/eclipse/eclipseC -noSplash -data ccsWorkspace -application com.ti.ccstudio.apps.projectBuild -ccs.buildType full -ccs.projects <my project>
Did anyone noticed similar issue?
Best regards,
David.