Hello
I'm currently using TI CC3200 LaunchPad and just trying to get used to it.
I'm using Win7 Professional 64 bit / CCS is at the latest version
Everything works great, I can use Uniflash, Energia, and CCS Debug ( with example projects) , and the programs are loaded, and run correctly.
But when using CCS and trying to program and debug an example, I notice that after the board is reset, the example is not stored anymore.
For example : Loaded an example with Energia. Then tried loading another example from the CCS (Blinky) . Blinky runs , but after I reset the board, the code that was written with Energia runs on the board.
Is my CCS code written only in the RAM memory?
Whan can I do to keep the CCS code after I reset the board?
I'm probably just doing something wrong but I've run out of ideas.
Console mesage after debug Blinky example project for cc3200:
Cortex_M4_0: GEL Output:
Memory Map Initialization Complete
Cortex_M4_0: GEL Output:
Target Reset
Thanks