Tool/software: Code Composer Studio
Hello,
I want to develop a gstreamer application in CCS6.2. From the command line I can compile and link my application with gstreamer with the following steps:
1. source the environment setup script:
source ~/ti-processor-sdk-linux-am57xx-evm-03.01.00.06/linux-devkit/environment-setup
2. Compile and Link:
arm-linux-gnueabihf-gcc -Wall helloworld.c -o helloworld $(pkg-config --cflags --libs gstreamer-1.0)
Sourcing the environment-setup script is necessary so that pkg-config finds the correct information about gstreamer libraries for ARM.
Now I want to compile out of CCS6.2. Where in CCS do I have to set the options shown above?
Thanks and have a nice day
Marc