Part Number: DRV8301-HC-C2-KIT
Tool/software: Code Composer Studio
Hi,
Can I Connect external pot to the drv 8301 for speed control. Can anyone suggest where to connect it to the DRV8301-HC-C2-KIT i.e., which pin and the terminal.
Thx
KVRao
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRV8301-HC-C2-KIT
Tool/software: Code Composer Studio
Hi,
Can I Connect external pot to the drv 8301 for speed control. Can anyone suggest where to connect it to the DRV8301-HC-C2-KIT i.e., which pin and the terminal.
Thx
KVRao
Dear Mr.Rick,
Thanks for the info. My program works fine with the inbuilt POT R28. Now I want to connect external pot without removing the R28 pot from the board.
I need to access any of the left over available ADC's. Please suggest.
thx
KVRao
Dear Mr.Rick,
Thanks for the info. To tap pin 65 of J1, I need to make a new board as the pin in not connected to any of the terminals.
Wondering if I could use Pin 38 of J5 to test the ext pot. The On board POT could be kept at home position.
Please suggest.
thx
KVRao