Hi,
One of our F28377D customer reported issue that when they group the CPU1 and CPU2 code and try to RUN them together it gives error. I reproduce this issue and found that issue occurs when code is running from FLASH. If the current PC is pointing to FLASH address when CPU is halted then running the cores using group option gives error. Look like it's not able to remove the breakpoint (which in this case would be HW breakpoint because FLASH can not written) and gives error. Strange thing is that I see this issue with XDS510 (from SD) emulator only and not with XDS100 emulator (tried only these two so far).
To reproduce this issue, please use import "blinky_dc" example from "controlSUITE\device_support\F2837xD\v190\F2837xD_examples_Dual"
Connect to CCS via XDS510 emulator. Group CPU1 and CPU2 like below -
Connect to both the core.
Change the build configuration of both the projects (CPU1 and CPU2) to *FLASH* and compile and load the respective .outs on CPU1 AND CPU2.
Now select "Group1" and click in "RUN" icon. You'll see the error.
Regards,
Vivek Singh