Other Parts Discussed in Thread: CC2650
Tool/software: Code Composer Studio
Hey guys,
I've imported several TI example projects and been extremely disappointed by their lack of functionality. They commonly don't work out of the box and most of my questions have been just getting these *example* projects to build, then debug properly. This isn't the first board I've worked with that had similar results. One of the previous examples I used had the wrong pins assigned to the uart module without documentation. I found and reported a couple pinout issues with the same board. I was hoping these instances were a thing of the past but I've since picked up a launchxl-cc2650 this obviously hasn't been fixed. I've tried several different sources for Project Zero for the CC2650. The only functioning version of it I was able to locate was in the cloud, but importing this project to my local machine caused a host of missing dependencies. Clearly this is an issue as I've located a couple sources mentioning a portability tutorial for TI code. I've got 3 versions of simplelink and 3 versions of RTOS now and I'm really not interested in expanding with more libraries and dependencies, especially since a lot of these also seem to contain broken links.
So my question is this: Are there any all-inclusive example projects for the CC2650 that do not depend on libraries (or include the file dependencies WITH the project download)? Are there any developers that have open source code posted to git for example?
Edit: As an alternative, if someone could follow the instructions here and zip up your working Project Zero I'd appreciate that as well.