Other Parts Discussed in Thread: UCD3138
Tool/software: Code Composer Studio
I am attempting to program a UCD3138A on my target PCB. When I compile the project and attempt to connect to the target with the TI USB Interface Adapter over PMBus, I get the following messages.
The memory map I am working through now, but more concerning to me is the "Trouble Reading Memory Block at 0x20 on Page 0 of Length 0x4: An error occurred accessing memory" error. I have the PMBus instrumented so that I can observe activity on the PMBus with an oscilloscope, but no activity occurs.
Do I need to use a JTAG adapter in place of the PMBus adapter for this type of debugging/programming?
ARM7_0: GEL Output: /nMemory Map Initialization Complete/nARM7_0: GEL Output: /tMemory Map Setup for Flash at Address 0x0ARM7_0: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
ARM7_0: Trouble Reading Memory Block at 0x20 on Page 0 of Length 0x4: An error occurred accessing memory
ARM7_0: File Loader: Verification failed: Target failed to read 0x00000020
ARM7_0: GEL: File: C:\DigitalPower\PSFBFirmware-1.1\PSFBFirmware-1.1\PSFB_PCM\UCD3138A\UCD3138_PSFB_PCM.out: Load failed.